ISerial::ReplacementCharacter
Description
Specifies the character to be used to replace incoming characters that arrive with errors (such as parity error.)
VB Prototype
Dim value As Byte
                                            value = object.ReplacementCharacter
                                        
object.ReplacementCharacter = value 
                                        
C++ Prototype
HRESULT get_ReplacementCharacter(
                                        
  BYTE* ReplacementCharacter
);
		
HRESULT put_ReplacementCharacter(
                                        
  BYTE ReplacementCharacter
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, BytesAvailable, BaudRate, DataBits, ClearToSendState, DataCarrierDetectState, DataSetReadyState, DataTerminalReadyState, EndIn, EndOut, FlowControl, Parity, RingIndicatorState, RequestToSendState, StopBits, ReplacementCharacter, XONCharacter, XOFFCharacter, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, SetBufferSize, Flush, ISerial Overview