STC/MIMO (IEEE 802.16 OFDMA)
The area of the Format tab contains parameters that control the operation of the STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively./MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. portion of the VSA. These parameters include:
Include Inactive Antenna Paths
See Also
Format Tab (IEEE 802.16 OFDMA)