Resource Map Length (Custom OFDM)
This parameter is shown in the Frame Definition tab. When Frame Definition > Apply is clicked, the value in the Frame Definition tab is applied to the Format tab (and the signal analysis results).
: 64 Symbols
sets the length in number of symbols used to create the Format tab resource mapping array properties (i.e. Resource Map, Resource Modulation and Resource Allocations) during the Frame Definition Apply process. The resource mapping array properties are created for the specified number of symbols based on the Frame Definition tab specified Frame Parts and Allocation Summary. If the result length is larger than length of the resource mapping arrays, the Resource Map Repeat Index is used to decide where to loop back in the resource mapping arrays after the end is reached.
See Also