Optional Measurement Software (Trace Data)
Optional measurement types typically add new trace data or modify the existing basic 89600 VSA trace data. Click on the following links to find out about specific optional measurement type trace data:
- 8960120xC/U Basic Vector Analysis and Hardware Connectivity
- 89601AYAC Vector Modulation Analysis
- 89601B7NC 3G Cellular Modulation Analysis
- 89601B7RC Wireless Connectivity Modulation Analysis
- 89601BHFC Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Modulation Analysis
- 89601BHGC LTE/LTE-A FDD Frequency Division Duplex: A duplex scheme in which uplink and downlink transmissions use different frequencies but are typically simultaneous. Modulation Analysis
- 89601BHHC LTE/LTE-A TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. Modulation Analysis
- 89601BHMC DOCSIS Modulation Analysis
- 89601BHNC 5G NR Modulation Analysis
- 89601BHPC FMCW Radar Analysis
- 89601BHQC Pulse Analysis
- 89601BHTC IoT Modulation Analysis
- 89601BHXC HT high throughput WLAN WLAN - Wireless Local Area Network: A system that includes the distribution system (DS), access points (APs), and portal entities. It is also the logical location of distribution and integration service functions of an extended service set (ESS). A WLAN system contains one or more APs and zero or more portals in addition to the DS. Modulation Analysis
- 89601DVBC Satellite Communications Modulation Analysis
See Also