Utilities Menu

The Utilities menu provides includes the following features:

This menu item…

Does this…

 

 

Macros...

Edit, record, and manage macros.

 

 

Event-Based Actions...

Define rules to perform actions based on measurement conditions.

 

 

Trend/Statistics...

Plot trend lines and statistical data within any measurement type.

 

 

General Preferences...

Configures settings that affect the general operation of the 89600 VSA software

 

 

SCPI Preferences...

Configure SCPI interface for controlling the 89600 VSA.

 

 

Display Preferences...

Configure the appearance of the VSA software's user interface including settings such as trace color, window theme and scaling, dialog behavior, and the User Color Map.

 

 

Toolbars...

Create custom toolbars and edit preconfigured toolbars.

 

 

Manage Registers...

Remove data registers.

 

 

Licenses...

Information about your license. The Keysight Software Manager Utility can be opened from here.

 

 

Extension Manager...

Choose which extensions to during at VSA startup.