Control tab (Source dialog)
Selecting opens the Source dialog Control tab. The Source Control tab provides all the controls and parameters required for VSA integrated control and operation of an external source.
You must first select a Source Configuration to enable the Source Control tab controls and parameters.
– Connects (or Disconnects) the Source Configuration. All parameters are disabled until you connect to the selected source configuration.
– Select either Physical or Logical. This is displayed only when the source channel configuration contains an I+jQ logical channel. It is not displayed when each source logical channel corresponds to a single physical source channel. When Physical channel view is selected and when Channel View is not shown, Source Channel selects channelized parameters on source physical channels. When Logical channel view is selected, Source Channel selects channelized parameters on logical channels.
– Some of the parameters in the tab are channelized, meaning each channel may have a different assigned value.
-
Selecting All populates channelized parameter values when all of the component carriers have the same assigned value. If one or more component carriers have differing values, "multiple values" will appear in the parameter's field.
Channelized parameters will display a drop-down icon to the right of the parameter. The color of the icon indicates the following:
-
Channelized parameter - All channels currently have the same assigned value for this parameter. -
Channelized parameter - Some channels currently have different values for this parameter.
You can also use the drop-down menu to change the tab's selected Source Channel (or all channels), which functions the same way as Source Channel.
-
-
Selecting an individual Source Channel will populate channelized parameters in the Control tab with the assigned values for just that channel.
If you are connected to a source that supports virtual signals, you can configure up to eight virtual signal generators per channel in the Download Waveform to Source area. See Supported Sources.
– Specifies the source carrier frequency for the selected Source Channel of a vector source generator. Displays the read-only downloaded waveform center frequency on a arbitrary waveform generator (AWG). When the source is an M8190A AWG with Option M8190A-DUC. RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). Frequency may be changed during playback of a downloaded waveform without reloading the waveform.
Shifts baseband frequency by the specified offset on source channels that support baseband frequency offset, such as M9415B.
– Specifies the incremental frequency step size for the keyboard arrow keys and mouse wheel. This setting applies to all channels. Not displayed when the source is an AWG because there is no carrier frequency to step.
– Specifies the source signal output power level for the selected Source Channel.
- When selected (true), sets the source "RF ON" parameter to ON, which turns on the source's RF output for the selected Source Channel.
– When selected (true), sets the vector source "Modulation ON" parameter to ON, which applies modulation to the carrier signal for the selected Source Channel. Modulation is always on with an AWG source; this property is not displayed.
– Specifies a time delay in seconds before playback begins on a waveform after playback is initiated. This property can be used to deskew source channels. Setting a value on All channels is most useful for resetting delay to zero on all channels. This property is supported for M8190A AWG. Changing delay on a waveform played with digital up conversion in Software trigger mode stops playback until a software trigger is sent.
– Specifies an offset in degrees on the carrier frequency set by digital up conversion of the downloaded waveform. Offset is in the range of ±180° within a period of the carrier frequency. This property is supported for M8190A AWG with Option M8190A-DUC and can be changed during playback. The value of this property is applied during waveform download to AWG models M8195A, M8198A, and M8199A.
– Specifies whether Single Ended or Differential output connection is selected. This is parameter is shown only when this selection is supported by the current source and source channel configuration.
Download Waveform to Source ("All" Source Channels selected)
– The center frequency that is applied to recorded data when downloading to an arbitrary waveform generator (AWG). Waveform Center Frequency has no effect with vector sources, so it is not displayed in the GUI with a vector source. It has an effect only when the source is an AWG and only during download. The value is applied to the arb waveform when generating the data downloaded to the AWG. Changing the value of Waveform Center Frequency has no effect until a download is performed. When using an AWG, after a download is performed, the Frequency property is set to the value of Waveform Center Frequency used during download.
Phase continuity of a waveform being played by an AWG depends on the relationship between the duration in time of the waveform being downloaded and the waveform center frequency. To maintain phase continuity while playing the waveform, the waveform center frequency in Hertz must be an integer multiple of the reciprocal of the waveform duration in seconds. The value of this property is rounded to the nearest frequency that maintains phase continuity when a waveform is downloaded. Frequency property is set to the rounded waveform center frequency applied to the downloaded waveform.
Waveform Center Frequency property is not supported with M8190A AWG. RF Frequency property is supported for setting waveform center frequency when M8190A-DUC is installed.
– Selects how the waveform will be adjusted when the waveform does not meet the source’s waveform length requirements. The available Waveform Adjustment choices depend on the model of source and its installed options.
Hover your mouse over the Waveform Adjustment drop-down box to see a pop up that displays the source length requirements, which includes the minimum waveform length and length quantum number.
-
Extend with Zeros – The ARB waveform is extended with zeros to meet the minimum waveform length (in points) and the waveform length quantum (length in points must be a multiple of the quantum) requirements. Note: this option does not ensure periodicity when the source is in Continuous playback.
When the source is an AWG and resampling is performed to obtain the AWG sample rate, the resampling filter is filled with zeros. When possible, the AWG sample rate is selected within the supported range of rates to avoid the need to extend with zeros. Otherwise, the ARB waveform is extended with zeros, which does not ensure periodicity when in Continuous playback.
VSA versions prior to VSA 2024 Update 2.0 used truncation to trim the waveform to meet the source's length quantum requirement (multiple of some number of samples). Truncation is no longer used because Extend with Zeros satisfies source requirements with no risk of data loss.
-
Ensure Periodicity – The ARB waveform is repeated, if necessary, to meet the minimum waveform length (in points) and the waveform length quantum (length in points must be a multiple of the quantum) requirements. This will ensure periodicity of the waveform in Continuous playback. For sources that support event/trigger out, there will be at least a trigger at the beginning of the repeated waveform, but not necessarily at each repetition. Note that for sources that don't support hardware-based repetition, this can increase the amount of data transferred to the source (affecting download speed and memory usage on the source).
When the source is an AWG and resampling is performed to obtain the AWG sample rate, the resampling filter is filled with values from the end of the ARB waveform to ensure periodicity.
-
Ensure Periodicity and Event Out – Same as Ensure Periodicity except that, for sources that support event/trigger out, there will be a trigger at each repetition of the waveform (if repetition needed).
When the source is an AWG and resampling is performed to obtain the AWG sample rate, the resampling filter is filled with values from the end of the ARB waveform to ensure periodicity.
– Displays the name of the last waveform file that was downloaded to the source. The Last Downloaded File field is updated whenever a new waveform file is downloaded to the source.
– This button, to the right of Last Downloaded file, repeats the download of the last downloaded current recording or file. A current recording is downloaded using the same measurement span and playback time parameters set for the last download. Redo Last Download is useful for applying a change in Waveform Center Frequency to the waveform played by an AWG. The button is not displayed until a download has been performed.
– It is displayed in the GUI only when supported. This property is supported with M8195A AWG. Event out markers are On by default for other sources that support downloading waveforms. M8195A markers are available for Channel 1. Marker 1 is output on Channel 3 and Marker 2 is output on Channel 4. When a M8195A source logical channel configuration contains Channel 3 or Channel 4 markers are not available. When Marker On property is set to Off, Channel 3 and Channel 4 are used only for waveform playback.
– Opens the Select dialog that is used to configure and download the current VSA measurement recording for ARB Source playback. See See "Using Source Download and Recording".
dialog options:
– The recording data in the current measurement span is downloaded instead of the entire recording span.
– The recording data is downloaded at the span when the recording was made.
– Downloads only the data between the playback start and stop times. See Specifying the Start/Stop region.
" and "", see Playback Tab (Recording).
– Downloads the entire recording.
When the recording is downloaded into the source, the center frequency is specified by the parameter (Hardware > Source Control tab), not the current VSA measurement center.
– Use Download File to select and download a VSA recorded signal file (VSA MATLAB ".mat" format) to an ARB Source for signal playback. See Source Signal Playback.
Each channel of a multi-channel waveform will be mapped to a different source channel if the mapping is 1:1. If a single-channel waveform is downloaded and multiple channels are enabled, the same waveform will be played on all enabled channels.
The order of the channels in the Channels tab is the same way channels will be ordered in the downloaded waveform.
- When checked, Sample Rate and RMS Power are set using values from the file or recording. When unchecked, the current values of Sample Rate and RMS Power are retained through the waveform download.
Download Waveform to Source (individual Source Channel selected)
– Selects how the waveform will be adjusted when the waveform does not meet the source’s waveform length requirements. The available Waveform Adjustment choices depend on the model of source and its installed options.
Hover your mouse over the Waveform Adjustment drop-down box to see a pop up that displays the source length requirements, which includes the minimum waveform length and length quantum number.
-
Extend with Zeros – The ARB waveform is extended with zeros to meet the minimum waveform length (in points) and the waveform length quantum (length in points must be a multiple of the quantum) requirements. Note: this option does not ensure periodicity when the source is in Continuous playback.
VSA versions prior to VSA 2024 Update 2.0 used truncation to trim the waveform to meet the source's length quantum requirement (multiple of some number of samples). Truncation is no longer used because Extend with Zeros satisfies source requirements with no risk of data loss.
-
Ensure Periodicity – The ARB waveform is repeated, if necessary, to meet the minimum waveform length (in points) and the waveform length quantum (length in points must be a multiple of the quantum) requirements. This will ensure periodicity of the waveform in Continuous playback. For sources that support event/trigger out, there will be at least a trigger at the beginning of the repeated waveform, but not necessarily at each repetition. Note that for sources that don't support hardware-based repetition, this can increase the amount of data transferred to the source (affecting download speed and memory usage on the source).
-
Ensure Periodicity and Event Out – Same as Ensure Periodicity except that, for sources that support event/trigger out, there will be a trigger at each repetition of the waveform (if repetition needed).
– All virtual signals in a source channel share the same available sample rate (for example, the M9494C VXG's available sample rate is 3.0 GHz Gigahertz: A frequency measurement which equals one billion hertz.). Each enabled virtual signal consumes a portion of the available sample rate. Remaining Sample Rate is the amount of the available sample rate that is not used by enabled virtual signals.
(only available when connected to a supported source)
| Virtual Signal | Enable | Sample Rate | RMS Power | Frequency Offset | Attenuation | Download Recording | Download File | Last Downloaded Waveform |
|---|---|---|---|---|---|---|---|---|
|
Index of the virtual signal (up to eight per channel) |
Enables the virtual signal. A virtual signal is enabled after its waveform is downloaded, unless the virtual signal’s sample rate exceeds Remaining Sample Rate. In this case, the waveform downloads but the virtual signal remains disabled. See Sample Rate for more information. |
Sample rate (Hz) for the virtual signal. Each enabled virtual signal consumes a portion of the available sample rate. A virtual signal with a downloaded waveform cannot be enabled if its sample rate exceeds the remaining sample rate. The Sample Rate entry of a virtual signal is highlighted in the table with a yellow border if its Enable checkbox is disabled because its sample rate value exceeds Remaining Sample Rate. |
RMS Power is a unitless ratio that sets the relationship between Total RMS Power (set by the source channel Amplitude property) and Peak Envelope Power, where PeakEnvelopePower (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) = TotalRMSPower (dBm) – ∑ [20 * log10(RMSPower)], with the sum of values from enabled virtual signals. By default, RMS Power is set when a waveform is downloaded using a value from the file or current recording data. A M9494C VXG Vector Signal Generator sets the power of each virtual signal so that the sum is Total RMS Power. However, the signal generator has a maximum peak power. The RMS Power value of each virtual signal may call for a Peak Envelope Power that exceeds what the signal generator can produce. This is indicated as an error condition in the signal generator user interface. |
Frequency Offset (Hz) for the virtual signal. The offset is the distance in frequency (Hz) from the channel’s RF center frequency to the center of the modulation bandwidth. |
Attenuation (dB) allows scaling a virtual signal down in amplitude. The dynamic range is not adjusted (optimized) when this value is adjusted. This virtual signal’s power relationship with other virtual signals, including noise, is not adjusted when this value is changed. The amount of attenuation applied is relative to the maximum of the Attenuation values of all enabled virtual signals. This property has no effect when only one virtual signal is enabled. |
Opens a dialog to configure and download the current VSA measurement recording to the virtual signal generator. |
Selects and downloads a VSA recorded signal file (VSA MATLAB ".mat" format) to the virtual signal generator. |
Displays the name of the last waveform file that was downloaded to the source. The full path name is displayed by the tooltip displayed when hovering the mouse over the text box. When a current recording is downloaded, <recording> is displayed. |
– When checked, Sample Rate and RMS Power are set using values from the file or recording. When unchecked, the current values of Sample Rate and RMS Power are retained through the waveform download.
Waveform Trigger
Waveform Trigger parameters are used to control triggering of downloaded waveforms.
The VSA software always uses Continuous trigger mode with sources that support Continuous and Single trigger modes.
Trigger controls are not displayed in the GUI when VSA does not support triggering for the source, or the source does not have trigger capabilities. See the Source Requirements topic for sources that support triggering.
Immediate – (Default) Waveform play starts as soon as a waveform is loaded and enabled.
Software– Waveform play starts when the Software Trigger button is clicked.
Global Trigger – Waveform play starts when the Global Trigger source trigger is asserted. Global Trigger starts repeatable, phase coherent waveform play. See the Source Requirements topic for sources that support Global Trigger.
Global Trigger Type
Immediate – (Default) Phase coherent waveform playback starts as soon as a waveform is loaded and enabled.
Software – Phase coherent waveform play starts when the Software Trigger button is clicked.
When Trigger Type is Immediate, a virtual signal’s markers are output as soon as the virtual signal is enabled. Setting Trigger Type to Software can be used to disable markers until all virtual signals are configured. Output of markers starts when Software Trigger is executed.
– Selects the action that is initiated by the trigger.
Run – Waveform play starts when trigger is received. Subsequent triggers are ignored.
Reset and Run – Waveform play starts when trigger is received. Subsequent trigger while waveform is playing will reset play to the start of the waveform. This mode is not supported for GlobalTrigger trigger type.
– Initiates a software trigger when the Trigger Type is set to Software.
Using Source Download and Recording
Using "Current" and "From File"
There are two Download Recording options: and :
Max Download File Size: The data block size to be downloaded to a source must be < 250 Mpts. The maximum data block size that can be downloaded to an AWG depends on the memory size of the AWG and the ratio between the sample rate in the recording file and the sample rate of the AWG. The length of the data will increase if it must be resampled to the AWG sample rate.
You will receive an ERROR message when the download a recording data size exceeds the source maximum memory size, see Reducing Download Recording Size.
Using "Download File..."
The option is used to browse, recall, and load a saved signal recording file for download and playback. This option allows you to save a measurement signal recording and recall it at a later time for detailed signal analysis. This feature also allows you to share a common signal recording file with multiple co-workers running the VSA software.
Using "Download Current Recording"
The option opens the Select dialog and is used to configure and download the current VSA measurement signal recording for playback. You do not need to download the entire signal recording for playback. For example, you may only want to do further signal analysis on a specific region (time interval) of the measurement recording.
Specifying the Start/Stop region
There are two methods for defining the recording download region (time interval) within the current measurement recording:
- You can use the Recording Playback "Start Time" and "Stop Time" parameters to specify the recording download playback region.
- You can open and use the recording Player (Acquisition > Player Window) to specify the download playback region. The graphical user interface makes it easy to visually identify the playback region of interest within the measurement recording.
Reducing Download Recording File Size
When you are downloading using the option, zooming in on a subset of the recording span and selecting “” will reduce both the sample rate and the amount of data downloaded (by the ratio of the current measurement span to the span of the recording). Selecting “” will reduce the amount of data downloaded but will not affect the sample rate.
I/Q Adjustments
I/Q Adjustment parameters are shown if the current source and source channel configuration supports any of the parameters described below. When supported, the Source Control tab may be extended to show I/Q Adjustment parameters.
– Specifies voltage offset applied to both I and Q signals. Common mode I/Q offset refers to the unwanted DC offset that appears equally in both the I and Q signals. This offset can originate from various sources, including mismatches in the analog components, such as digital-to-analog converters (DACs), or imperfections in the signal generation process. This offset can affect the quality of the generated signal by introducing errors in the modulation, leading to issues such as increased error vector magnitude (EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format.) and degraded signal fidelity. This parameter is shown only when supported by the current source and source channel configuration.
– Specifies whether the supported adjustment parameters below are applied in the source.
– Specifies amplitude imbalance correction in dB between I and Q signals that preserves the composite magnitude.
– Specifies an absolute phase adjustment in degrees of both I and Q signals which adjusts relative RF carrier phase.
– Specifies timing skew correction in seconds between I and Q signals.
– Specifies delay adjustment of both I and Q signals relative to markers.
– Specifies correction in degrees for deviation of I/Q angle from 90°.
– Specifies DC offset correction for the I signal as a percentage of ARB waveform RMS voltage.
- Specifies DC offset correction for the Q signal as a percentage of ARB waveform RMS voltage.
See Also
Using MATLAB Simulated Signals