PayLoad Octet Calculations  (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Time tab

PayLoad Octets specify the number of payload data bits (in units of Octets) included for measurement analysis. The PayLoad Octets determine the measurement packet length, the length of the Packet Time trace and Packet Spectrum trace data. A PayLoad Octets value of 0 (default) represents a packet consisting of the 12 Header symbol-times and 0 Payload symbol-times.

PayLoad Octets is a function of Result Length and Data Rate. Changing the  Result Length setting will cause the number of PayLoad Octets to be changed and changing PayLoad Octets will cause the Result Length to be changed.

PayLoad Octet Calculation

The ceiling function forumula is used to calculate the PayLoad Octets:

where: Payload Symbols = Result Length -12, and

            InfoBits value is provided in the Data Rates table.

MB-OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Data Rate Parameters

Data Rate (Mb/sec)

Modulation Type

Coding Rate

FDS

TDS

Coded Bits*

Info Bits*

Preamble

53.3

QPSK Quadrature phase shift keying

1/3

Yes

Yes

300

100

Standard

80.0

QPSK

1/2

Yes

Yes

300

150

Standard

106.7

QPSK

1/3

No

Yes

600

200

Standard

160.0

QPSK

1/2

No

Yes

600

300

Standard

200.0

QPSK

5/8

No

Yes

600

375

Standard

320.0

DCM

1/2

No

No

1200

600

Standard/
Burst

400.0

DCM

5/8

No

No

1200

750

Standard/
Burst

480.0

DCM

3/4

No

No

1200

900

Standard/
Burst

* Per (6) OFDM Symbols

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Format Tab (MB-OFDM Demod Properties)

Time Tab (MB-OFDM Demod Properties)

Advanced Tab (MB-OFDM Demod Properties)