Invert (RFID)
: Unselected (See RFID Standard Setups/Presets Table)
The inverts the raw demod bits prior to line decoding. This signal inversion can be required because at higher bit rates ISO 18092 allows signals passing in either direction to have reverse Manchester encoding.
See Also
Format Tab (RFID Demod Properties)