Points / Symbol
: 20 (See RFID Standard Setups/Presets Table)
10, 20, 50, 100
The text box sets the number of points per symbol for the and traces. Available settings are 10, 20, 50, and 100.
When either or is set to , the upper limit of is 20.
See Also
Format Tab (RFID Demod Properties)
Demod Meas Time With CW (RFID)