Basic Midamble (TD-SCDMA)
0 (See TD-SCDMA Standard Setups/Presets Table.)
: 0 to 127
specifies the training sequences for uplink and downlink channel estimation, power measurements and maintaining uplink synchronization (see TD-SCDMA - Code/ID Allocation Overview ).
: Controls the allowable Basic Midamble ID sequence coding criteria as follows:
: Only allows Basic Midamble ID sequences that comply with standard coding allocation criteria.
: Allows non-standard Basic Midamble ID sequence allocation.
See Also