|
(Read-Write) Set and query the EMI mode's Amplitude Probability Distribution (APD) statistics 6 dB resolution bandwidth i.e., available when MEAS is set to SAPD). See also, MEAS, CISP:BAND, FREQ:AXIS:LOG, BAND:EMI:AUTO, BAND:EMI:RES, SWE:EMI:DWEL, BAND:APD:AUTO, SWE:EMI:DWEL, EDET:TRAC, TRAC<v>:APD:INPUT. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<num> |
Resolution Bandwidth in Hz. Dynamic. Varies with EMI band set. See also, CISP:BAND. This command will accept MIN and MAX as arguments. |
|
Examples |
BAND:APD 10e3 'Sets APD statistics 6 dB resolution bandwidth to 10e3 |
|
Query Syntax |
[:SENSe]:BANDwidth:APD[:RESolution]? |
|
Return Type |
Numeric |
|
Default |
1.200000E+05 (at preset; else, varies by EMI band selected) |
Last Modified:
|
31-Aug-2023 |
New command (A12.3x) |