(Read-Write) Set and query the status of the active EMI (electromagnetic interference) band scan type. See also, CISP:BAND, FREQ:AXIS:LOG, BAND:EMI, BAND:EMI:AUTO, BAND:APD:RES, SWE:EMI:DWEL, BAND:APD:AUTO, SWE:EMI:DWEL, EDET:TRAC, TRAC<v>:APD:INPUT. |
|
Relevant Modes |
|
Parameters |
|
<char> |
Choose from: FPSC (Default) - Sets the EMI scan to Fast SA Scan (FPSCan). CBSC - Sets the EMI scan to EMI Band Scan (CBSCan). CZSC - Sets the EMI scan to EMI Zero Scan (CZSCan). SAPD - Sets the EMI scan to Amplitude Probability Distribution (APD) statistics scan. |
Examples |
MEAS CBSC 'Sets the EMI scan to EMI band scan (i.e., standard EMI band scan). MEAS CZSC 'Sets the EMI scan to Zero scan. MEAS CZSC 'Sets the EMI scan to APD statistics scan. |
Query Syntax |
MEASure? |
Return Type |
character |
Default |
FPSC |
Last Modified:
22-044-2026 |
New command (A.12.3x) |