|
(Read-Write) Set and query the status of the EMI mode's active CISPR band being measured . See also, MEAS, FREQ:AXIS:LOG, BAND:EMI, BAND:EMI:AUTO, BAND:APD:RES, SWE:EMI:DWEL, BAND:APD:AUTO, SWE:EMI:DWEL, EDET:TRAC, TRAC<v>:APD:INPUT. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Choose from: A - Sets the EMI CISPR band to A band (9k - 150 kHz). B - Sets the EMI CISPR band to B band (150k - 30 MHz). C (Default) - Sets the EMI CISPR band to C band (30M - 300 MHz). D - Sets the EMI CISPR band to D band (300M - 1 GHz). E - Sets the EMI CISPR band to E band (1G - 18 GHz). |
|
Examples |
CISP:BAND A 'Sets A band as the EMI CISPR active band being measured. CISP:BAND E 'Sets E band as the EMI CISPR active band being measured.. |
|
Query Syntax |
CISP:BAND? |
|
Return Type |
character |
|
Default |
C |
Last Modified:
|
31-Aug-2023 |
New command (A.12.3x) |