(Read-Write) Set and query the Amplitude Probability Distribution (APD) satistics settling time after the internal source steps to the next frequency and before the power sensor makes a measurement (i.e., only available when MEAS is set to SAPD ). See also, MEAS, CISP:BAND, FREQ:AXIS:LOG, BAND:APD:RES, BAND:EMI:RES, BAND:EMI:AUTO, BAND:APD:AUTO, SWE:EMI:DWEL, EDET:TRAC, TRAC<v>:APD:INPUT. |
|
Relevant Modes |
EMI (Opt 361) |
Parameters |
|
<value> |
Dwell time in seconds. (Range: 10 ms to 120 seconds) |
Examples |
SWE:APD:DWEL .010 'sets the APD statistics dwell to 10 ms. |
Query Syntax |
[:SENSe]:SWE:APD:DWELl? |
Return Type |
Numeric |
Default |
1.000E-01 |
Last Modified:
22-044-2026 |
New command |