[:SENSe]:SWEep:EMI:DWELl <value>

(Read-Write) Set and query the settling time after the internal source steps to the next frequency and before the power sensor makes a measurement (i.e., only available when MEAS is set to CBSCan | CZSCan ).

See also, MEAS, CISP:BAND, FREQ:AXIS:LOG, BAND:APD:RES, BAND:EMI:RES, BAND:EMI:AUTO, BAND:APD:AUTO, SWE:APD:DWEL, EDET:TRAC, TRAC<v>:APD:INPUT.

Relevant Modes

EMI (Opt 361)

Parameters

 

<value>

Dwell time in seconds. (Range: 1 ms to 11 seconds)

Examples

SWE:EMI:DWEL .001 'sets the EMI band dwell to 1 ms.

Query Syntax

[:SENSe]:SWE:EMI:DWELl?

Return Type

Numeric

Default

1.000E-01


Last Modified:

22-044-2026

New command