|
(Read-Write) Set and query the EMI mode's Amplitude Probability Distribution (APD) statistics automatic resolution bandwidth state (i.e., available when MEAS is set to SAPD). See also, MEAS, CISP:BAND, FREQ:AXIS:LOG, BAND:APD:RES, BAND:EMI:RES, BAND:EMI:AUTO, SWE:EMI:DWE, BAND:APD, SWE:EMI:DWEL, EDET:TRAC, TRAC<v>:APD:INPUT. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<bool> |
Choose from: O or OFF - Set APD statistics Resolution BW manually using: BAND:APD:RES <num>. 1 or ON - Set APD (Automatic) statistics Resolution Bandwidth setting. |
|
Examples |
BAND:APD:AUTO 0 |
|
Query Syntax |
[:SENSe]:BANDwidth:APD[:RESolution]:AUTO? |
|
Return Type |
Boolean |
|
Default |
1 (ON) |
Last Modified:
|
31-Aug-2023 |
New command |