(Read-Write) Set and query the SEM carrier definition (i.e., from the Carrier Center (FCC) or from the Carrier Edge (FCE)). See also SEM:OFFS<n>:BAND:AUTO, SEM:OFFS<n>:BAND, SEM:OFFS<n>:ENAB, SEM:OFFS<n>:FREQ:STAR, SEM:OFFS<n>:FREQ:STOP, and SEM:OFFS<n>:SIDE. |
|
Relevant Modes |
|
Parameters |
|
<char> |
SEM Carrier reference. Choose from: FCC - Carrier Center is used for the SEM FCE - Carrier Edge is used for the SEM |
Examples |
SEM:OFD FCE 'the Carrier Edge is used as the SEM center |
Query Syntax |
SEM:OFD? |
Return Type |
Character |
Default |
FCC |
Last Modified:
01dec2019 |
Added SEM parameter |