[:SENSe]:SEMask:OFFSet<n>:BANDwidth[:RESolution]  <num>

(Read-Write) Set and query the SEM offset resolution BW for the selected channel (1 through 8). 

See also SEM:OFD, SEM:OFFS<n>:BAND:AUTO, SEM:OFFS<n>:ENAB,  SEM:OFFS<n>:FREQ:STAR,  SEM:OFFS<n>:FREQ:STOP, and SEM:OFFS<n>:SIDE.

Relevant Modes

SA

Parameters

 

<numeric>

Choose from:

Enter a channel number from 1 through 8.

<numeric>

Set the Resolution BW. Choose from:

10 | 30 | 100 | 300 | 1000 | 3000 | 10000 | 30000 | 100000 | ... | 5 MHz

Accepts MINimum and MAXimum as commands.

Examples

SEM:OFFS7:BAND 30000 'Sets the SEM channel 7 to a offset resolution BW of 30 kHz.

Query Syntax

SEM:OFFS5:BAND?

Return Type

numeric

Default

Dynamic: model/option dependent


Last Modified:

01dec2019

New command