(Read-Write) Set and query the type of SEM Offset to be activated (BOTH, just NEGative slope, or just the POSitive slope). See also SEM:OFD, SEM:OFFS<n>:BAND:AUTO, SEM:OFFS<n>:ENAB, SEM:OFFS<n>:FREQ:BAND, SEM:OFFS<n>:FREQ:STARt, and SEM:OFFS<n>:STOP. |
|
Relevant Modes |
|
Parameters |
|
<numeric> |
Choose from: Enter a channel number from 1 through 8. |
<character> |
Choose from: BOTH- Selects the SEM Offset to include both the negative (lower) and positive (upper) frequencies to display. NEG- Selects the SEM Offset to include only the negative (lower) frequencies to display. POS - Selects SEM Offset to include only the postive (upper) frequencies to display. |
Examples |
SEM:OFFS7:SIDE POS 'Sets the channel 7 SEM Offset side to be positive (upper). SEM:OFFS:SIDE BOTH'Sets the channel 1 SEM Offset to display both positive and negative frequencies. |
Query Syntax |
SEM:OFFS5:SIDE? |
Return Type |
Character |
Default |
BOTH |
Last Modified:
01dec2019 |
New command |