[:SENSe]:SEMask:OFFSet<n>:BANDwidth[:RESolution]:AUTO <bool>

(Read-Write) Set and query the SEM offset resolution BW Auto setting.

See also SEM:OFD, SEM:OFFS<n>:BAND, SEM:OFFS<n>:ENAB,  SEM:OFFS<n>:FREQ:STAR,  SEM:OFFS<n>:FREQ:STOP, and SEM:OFFS<n>:SIDE.

Relevant Modes

SA

Parameters

 

<numeric>

Choose from:

Enter a channel number from 1 through 8.

<booleon>

Choose from:

OFF (0) - SEM offset resolution BW Auto control is disabled.

ON (1) - SEM offset resolution BW Auto control is enabled.

Examples

SEM:OFFS7:BAND:AUTO 0 'disables the SEM offset resolution BW Auto setting.

Query Syntax

SEM:OFF5:AUTO?

Return Type

numeric

Default

<n> = 1

Offset Res BW = OFF(0)


Last modified:

01dec2019

Added to SA