(Read-Write) Set and query the SEM frequency Offset state. See also SEM:OFD, SEM:OFFS<n>:BAND:AUTO, SEM:OFFS<n>:BAND, SEM:OFFS<n>:FREQ:STAR, SEM:OFFS<n>:FREQ:STOP, and SEM:OFFS<n>:SIDE. |
|
Relevant Modes |
|
Parameters |
|
<booleon> |
Choose from: OFF (0) - Offsets are disabled. ON (1) - Offsets are enabled. |
Examples |
SEM:OFFS7:ENAB 0 'disables SEM freqeuency offsets for channel 7 SEM:OFFS:ENAB ON 'enables SEM freqeuncy offsets for channel 1 |
Query Syntax |
SEM:OFFS:ENAB? |
Return Type |
numeric |
Default |
1 |
Last modified:
01dec2019 |
Added to SA |