Specifies the settings to remotely control the rear panel connectors, an external test set, Calpod modules, and ECal Module state.
CONTrol CHANnel:INTerface:CONTrol: | [STATe] ECAL:MODule: | PATH: | COUNt? | STATe | STATe EXTernal:TESTset - More Commands | TRIGger | ATBA | OUTP |
Click on a keyword to view the command details.
Blue command is superseded.
See Also
See a pinout and detailed description of the rear panel connectors:
(Write-Read) Sends commands that control a Calpod module. Reads query versions Calpod commands. See ALL Calpod commands. |
|
Parameters |
|
<string> |
Calpod command. See ALL Calpod commands that can be used in this string. |
Write Example |
CONT:CALP:COMM 'CALP:INIT:ACT' 'Enclose all strings in SINGLE quotes (NOT double quotes) |
Query Syntax |
CONTrol:CALPod:COMMand? <string> Relevant only for query strings. |
Read Example |
CONT:CALP:COMM? '*OPC?' 'returns 0 if the calpod software is currently processing an operation 'returns 1 if operations are complete |
Return Type |
String |
Not Applicable |
|
(Write-only) Recalls an Interface Control configuration file. Learn more about Interface Control. |
|
Parameters |
|
<string> |
File name and extension (.xml) of the configuration file to recall. Files are typically stored in the default folder "C:/Program Files/Keysight/Network Analyzer/Documents". To recall from a different folder, specify the full path name. |
Examples |
CONT:CHAN:INT:CONT:CONF:REC 'MyConfigFile.xml' control:channel:interface:control:config:recall:state 'c:\users\public\documents\Network analyzer\Documents\MyFile.xml' |
Query Syntax |
Not Applicable |
Not Applicable |
|
(Read-Write) Enables and disables ALL Interface Control settings. To send data, the individual interfaces must also be enabled. Learn more about Interface Control. |
|
Parameters |
|
<bool> |
Boolean OFF (0) - Interface Control is disabled;NO control data is sent. ON (1) - Interface Control is enabled. |
Examples |
CONT:CHAN:INT:CONT 1 control:channel:interface:control:state 0 |
Query Syntax |
CONTrol:CHANnel:INTerface:CONTrol[:STATe]? |
Return Type |
Boolean |
OFF (0) |
|
(Read-only) Returns the number of unique states that exist for the specified path name on the selected ECal module. This command performs exactly the same function as SENS:CORR:CKIT:ECAL:PATH:COUNt? Use the CONT:ECAL:MOD:PATH:STAT command to set the module into one of those states. Use SENS:CORR:CKIT:ECAL:PATH:DATA? to read the data for a state. |
|
Parameters |
|
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
<name> |
Name of the path for which to read number of states. Choose from: Reflection paths
Transmission paths
Note: For each transmission path, the first of the available states is the through state, the second is the confidence (attenuator) state. |
Examples |
CONT:ECAL:MOD:PATH:COUNt? A control:ecal:module2:path:count? cd |
Return Type |
Integer |
Not Applicable |
|
(Write-only) Sets the internal state of the selected ECAL module. This command supersedes CONT:ECAL:MOD:STAT.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Parameters |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<path> |
Path name for which to set a state. Note: The impedance paths are not independent. For example, changing the impedance presented on path A will cause a change to the impedance on path B. Choose from: Reflection paths
Transmission paths
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<stateNum> |
Number of the state to set. Refer to the following table to associate the <stateNum> with a state in your ECal module. In addition, CONT:ECAL:MOD:PATH:COUNt? returns the number of states in the specified ECal module.
** The following modules have only FOUR Impedance states (1, 2, 3, 4): N4690B ,N4691B ,N4692A ,N4696B, N7550A - N7556A. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Examples |
CONT:ECAL:MOD:PATH:STATe A,5 control:ecal:module2:state BC,1 |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Query Syntax |
Not Applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Not Applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This command is replaced with CONT:ECAL:MOD:PATH:STATe. (Write-only) Sets the internal state of the selected ECAL module. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Parameters |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:COLL:CKIT:INF? to verify their identity. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<value> |
Integer code for switching the module. The following are codes for Keysight ECal modules.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Examples |
CONT:ECAL:MOD:STAT
36 |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Query Syntax |
Not Applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Not Applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
(Read-Write) Set and read the noise source (28V) ON and OFF. |
|
Parameters |
|
<bool> |
Boolean OFF (0) - Noise Source OFF ON (1) - Noise Source ON |
Examples |
CONT:NOIS:SOUR 1 control:noise:source:state 0 |
Query Syntax |
CONTrol:NOISe:SOURce[:STATe]? |
Return Type |
Boolean |
For PNA models with a Noise Figure option (028/029/H29), the 28V line is ON at application start and after a preset. The ON/OFF state is also available from a PNA softkey menu. For PNA models WITHOUT a Noise Figure option (028/029/H29), the 28V line is OFF at application start and its state is not affected by a preset. The ON/OFF state is NOT available from a PNA softkey menu. |
|
(Read-Write) Configures external triggering in the PNA. Note: To configure external triggering in the current PNA models, use the Trigger commands.
|
|
Parameters |
|
<conn> |
Rear Panel connector to send or receive trigger signals. Choose from: BNC1 Trigger IN from rear-panel Trigger IN BNC connector Note: Only one of the input connectors is active at a time. When a command is sent to one, the PNA automatically makes the other INACTIVE. BNC2 Trigger OUT to rear-panel Trigger OUT BNC connector. MATHtrigger - Trigger IN from rear-panel Material Handler connector Pin 18 RDY - Ready for trigger OUT.
|
<char> |
INACTIVE - Disables the specified connector <conn>. Choose from ONLY the following when <conn> is set to BNC1 or AUXT or MATHtrigger:
Choose from ONLY the following when <conn> is set to BNC2: Use CONTrol:SIGNal:TRIGger:OUTP to enable the BNC2 output. The following selections send a positive or negative pulse before or after each trigger acquisition. This normally occurs each sweep unless a channel is in point trigger mode.
Choose from ONLY the following when <conn> is set to RDY:
|
Examples |
CONT:SIGN
BNC1,TIENEGATIVE CONT:SIGN RDY,LOW |
Query Syntax |
CONTrol:SIGNal? <conn> In addition to the arguments listed above, the following is also a possible returned value: NAVAILABLE - This feature is not available on this PNA |
Return Type |
Character |
At Preset: BNC1 = INACTIVE When Output is enabled: BNC1 = INACTIVE |
|
(Read-Write) Accept Trigger Before Armed Determines what happens to an EDGE trigger signal if it occurs before the PNA is ready to be triggered. (LEVEL trigger signals are always ignored.) For more information, see External triggering. |
|
Parameters |
|
<bool> |
Boolean OFF (0) - A trigger signal is ignored if it occurs before the PNA is ready to be triggered. ON (1) - A trigger signal is remembered and then used when the PNA becomes armed (ready to be triggered). The PNA remembers only one trigger signal. |
Examples |
CONT:SIGN:TRIG:ATBA
0 |
Query Syntax |
CONTrol:SIGNal:TRIGger:ATBA? |
Return Type |
Boolean |
OFF |
|
(Read-Write) Output Enabled The PNA can be enabled to send trigger signals out the rear-panel TRIGGER OUT BNC connector. Use CONTrol:SIGNal to configure for output triggers. Note: To configure external triggering in the current PNA models, use the Trigger commands. For more information, see External triggering. |
|
Parameters |
|
<bool> |
Boolean OFF (0) - PNA does NOT output trigger signals. ON (1) - PNA DOES output trigger signals. |
Examples |
CONT:SIGN:TRIG:OUTP 1 control:signal:trigger:outp OFF |
Query Syntax |
CONTrol:SIGNal:TRIGger:OUTP? |
Return Type |
Boolean |
OFF |
|