:CRECovery:CEIDle

Command Syntax

:CRECovery:CEIDle {ON | OFF | 1 | 0}

Query Syntax

:CRECovery:CEIDle?

Description

Enables or disables the Contains Electrical Idle option.

When you are decoding a serial bus that has bursts of serial data followed by long periods of idle time, enabling the Contains Electrical Idle control will remove idle time from the decoded serial data.

To specify the Idle Clock Count, use :CRECovery:ICCount.