:CRECovery:ECLock:DELay
CRECovery Global Commands
- :CRECovery Subsystem
- :CRECovery:CEALgorithm
- :CRECovery:CEIDle
- :CRECovery:CFRequency:EDIRection
- :CRECovery:CFRequency:MODE
- :CRECovery:CSKew
- :CRECovery:DDRFive:CAFLatency
- :CRECovery:DDRFive:CAFSource
- :CRECovery:DDRFive:DQSSource
- :CRECovery:DDRFive:POLength
- :CRECovery:DDRFive:PRLength
- :CRECovery:DDRFive:RWMode
- :CRECovery:DDRFive:STDDelay
- :CRECovery:DREMoval
- :CRECovery:ECLock:ALIGn
- :CRECovery:ECLock:CFRequency
- :CRECovery:ECLock:CMULtiplier
- :CRECovery:ECLock:DELay
- :CRECovery:ECLock:EDIRection
- :CRECovery:ECLock:SOURce
- :CRECovery:FOPLl:LBANdwidth
- :CRECovery:FOPLl:LBDivisor
- :CRECovery:ICCount
- :CRECovery:MODE
- :CRECovery:PLL:EDIRection
- :CRECovery:PLL:MODE
- :CRECovery:PLL:SSCCorrect
- :CRECovery:PLL:SSPercent
- :CRECovery:PLL:SSType
- :CRECovery:PLL:STIMe
- :CRECovery:PLL:TDEPendent
- :CRECovery:PRESets
- :CRECovery:PRESets:SELections?
- :CRECovery:SOPLl:JTF:LBANdwidth
- :CRECovery:SOPLl:JTF:LBDivisor
- :CRECovery:SOPLl:JTF:PEAKing
- :CRECovery:SOPLl:OJTF:DFACtor
- :CRECovery:SOPLl:OJTF:LBANdwidth
- :CRECovery:SOPLl:OJTF:LBDivisor
- :CRECovery:SRATe
- :CRECovery:TOPLl:DFACtor
- :CRECovery:TOPLl:NFReq
- :CRECovery:TOPLl:PFReq
- :CRECovery:ZOPLl:LFPole
- :CRECovery:ZOPLl:PPOLe
- :CRECovery:ZOPLl:SPOLe
Command Syntax
:CRECovery:ECLock:DELay <seconds>
<seconds> is a real number time value in seconds.
Query Syntax
:CRECovery:ECLock:DELay?
Description
When an Explicit clock recovery method is selected (see :CRECovery:MODE), this command specifies a delay that is added to each of the clock times. For example, entering 1 ps will add 1 ps to each of the clocks recovered from the explicit clock source.