:CRECovery:ICCount

Command Syntax

:CRECovery:ICCount <idle_clock_count>

<idle_clock_count> is an integer from 10 to 200.

Query Syntax

:CRECovery:ICCount?

Description

When Contains Electrical Idle is enabled (see :CRECovery:CEIDle), this command specifies the number of clock periods without a data transition (edge) that indicate an idle condition. This option lets protocol decoders suppress decode for idle data periods on serial data links that go quiescent for a period of time and then restart transmitting.

Example Command Sequence

:CRECovery:MODE FOPLl
:CRECovery:CEIDle ON
:CRECovery:ICCount 80