:CRECovery:ECLock:CFRequency
CRECovery Global Commands
- :CRECovery Subsystem
- :CRECovery:CEALgorithm
- :CRECovery:CEIDle
- :CRECovery:CFRequency:EDIRection
- :CRECovery:CFRequency:MODE
- :CRECovery:CSKew
- :CRECovery:DDRFive:CAFLatency
- :CRECovery:DDRFive:CAFSource
- :CRECovery:DDRFive:DQSSource
- :CRECovery:DDRFive:POLength
- :CRECovery:DDRFive:PRLength
- :CRECovery:DDRFive:RWMode
- :CRECovery:DDRFive:STDDelay
- :CRECovery:DREMoval
- :CRECovery:ECLock:ALIGn
- :CRECovery:ECLock:CFRequency
- :CRECovery:ECLock:CMULtiplier
- :CRECovery:ECLock:DELay
- :CRECovery:ECLock:EDIRection
- :CRECovery:ECLock:SOURce
- :CRECovery:FOPLl:LBANdwidth
- :CRECovery:FOPLl:LBDivisor
- :CRECovery:ICCount
- :CRECovery:MODE
- :CRECovery:PLL:EDIRection
- :CRECovery:PLL:MODE
- :CRECovery:PLL:SSCCorrect
- :CRECovery:PLL:SSPercent
- :CRECovery:PLL:SSType
- :CRECovery:PLL:STIMe
- :CRECovery:PLL:TDEPendent
- :CRECovery:PRESets
- :CRECovery:PRESets:SELections?
- :CRECovery:SOPLl:JTF:LBANdwidth
- :CRECovery:SOPLl:JTF:LBDivisor
- :CRECovery:SOPLl:JTF:PEAKing
- :CRECovery:SOPLl:OJTF:DFACtor
- :CRECovery:SOPLl:OJTF:LBANdwidth
- :CRECovery:SOPLl:OJTF:LBDivisor
- :CRECovery:SRATe
- :CRECovery:TOPLl:DFACtor
- :CRECovery:TOPLl:NFReq
- :CRECovery:TOPLl:PFReq
- :CRECovery:ZOPLl:LFPole
- :CRECovery:ZOPLl:PPOLe
- :CRECovery:ZOPLl:SPOLe
Command Syntax
:CRECovery:ECLock:CFRequency <frequency>
<frequency> is a real number used for the clock frequency of the PLL.
Query Syntax
:CRECovery:ECLock:CFRequency?
Description
With the Explicit 1st or 2nd Order PLL clock recovery methods (see :CRECovery:MODE), this command specifies the clock frequency of the PLL.
Example Command Sequence
:CRECovery:MODE EFOPll :CRECovery:ECLock:CFRequency 1.485E+09