:CRECovery:PLL:STIMe
CRECovery Global Commands
- :CRECovery Subsystem
- :CRECovery:CEALgorithm
- :CRECovery:CEIDle
- :CRECovery:CFRequency:EDIRection
- :CRECovery:CFRequency:MODE
- :CRECovery:CSKew
- :CRECovery:DDRFive:CAFLatency
- :CRECovery:DDRFive:CAFSource
- :CRECovery:DDRFive:DQSSource
- :CRECovery:DDRFive:POLength
- :CRECovery:DDRFive:PRLength
- :CRECovery:DDRFive:RWMode
- :CRECovery:DDRFive:STDDelay
- :CRECovery:DREMoval
- :CRECovery:ECLock:ALIGn
- :CRECovery:ECLock:CFRequency
- :CRECovery:ECLock:CMULtiplier
- :CRECovery:ECLock:DELay
- :CRECovery:ECLock:EDIRection
- :CRECovery:ECLock:SOURce
- :CRECovery:FOPLl:LBANdwidth
- :CRECovery:FOPLl:LBDivisor
- :CRECovery:ICCount
- :CRECovery:MODE
- :CRECovery:PLL:EDIRection
- :CRECovery:PLL:MODE
- :CRECovery:PLL:SSCCorrect
- :CRECovery:PLL:SSPercent
- :CRECovery:PLL:SSType
- :CRECovery:PLL:STIMe
- :CRECovery:PLL:TDEPendent
- :CRECovery:PRESets
- :CRECovery:PRESets:SELections?
- :CRECovery:SOPLl:JTF:LBANdwidth
- :CRECovery:SOPLl:JTF:LBDivisor
- :CRECovery:SOPLl:JTF:PEAKing
- :CRECovery:SOPLl:OJTF:DFACtor
- :CRECovery:SOPLl:OJTF:LBANdwidth
- :CRECovery:SOPLl:OJTF:LBDivisor
- :CRECovery:SRATe
- :CRECovery:TOPLl:DFACtor
- :CRECovery:TOPLl:NFReq
- :CRECovery:TOPLl:PFReq
- :CRECovery:ZOPLl:LFPole
- :CRECovery:ZOPLl:PPOLe
- :CRECovery:ZOPLl:SPOLe
Command Syntax
:CRECovery:PLL:STIMe <settling_time>
<settling_time> is a double.
Query Syntax
:CRECovery:PLL:STIMe?
Description
Specifies the settling time as a number of time constants. All PLLs take a finite amount of time to lock on to their source signal. During this settling time portion of the acquisition record, jitter measurements, protocol decode, etc. will not be performed.
Example Command Sequence
:CRECovery:MODE FOPLl :CRECovery:PLL:STIMe 5.0