:CRECovery:PLL:EDIRection
CRECovery Global Commands
- :CRECovery Subsystem
- :CRECovery:CEALgorithm
- :CRECovery:CEIDle
- :CRECovery:CFRequency:EDIRection
- :CRECovery:CFRequency:MODE
- :CRECovery:CSKew
- :CRECovery:DDRFive:CAFLatency
- :CRECovery:DDRFive:CAFSource
- :CRECovery:DDRFive:DQSSource
- :CRECovery:DDRFive:POLength
- :CRECovery:DDRFive:PRLength
- :CRECovery:DDRFive:RWMode
- :CRECovery:DDRFive:STDDelay
- :CRECovery:DREMoval
- :CRECovery:ECLock:ALIGn
- :CRECovery:ECLock:CFRequency
- :CRECovery:ECLock:CMULtiplier
- :CRECovery:ECLock:DELay
- :CRECovery:ECLock:EDIRection
- :CRECovery:ECLock:SOURce
- :CRECovery:FOPLl:LBANdwidth
- :CRECovery:FOPLl:LBDivisor
- :CRECovery:ICCount
- :CRECovery:MODE
- :CRECovery:PLL:EDIRection
- :CRECovery:PLL:MODE
- :CRECovery:PLL:SSCCorrect
- :CRECovery:PLL:SSPercent
- :CRECovery:PLL:SSType
- :CRECovery:PLL:STIMe
- :CRECovery:PLL:TDEPendent
- :CRECovery:PRESets
- :CRECovery:PRESets:SELections?
- :CRECovery:SOPLl:JTF:LBANdwidth
- :CRECovery:SOPLl:JTF:LBDivisor
- :CRECovery:SOPLl:JTF:PEAKing
- :CRECovery:SOPLl:OJTF:DFACtor
- :CRECovery:SOPLl:OJTF:LBANdwidth
- :CRECovery:SOPLl:OJTF:LBDivisor
- :CRECovery:SRATe
- :CRECovery:TOPLl:DFACtor
- :CRECovery:TOPLl:NFReq
- :CRECovery:TOPLl:PFReq
- :CRECovery:ZOPLl:LFPole
- :CRECovery:ZOPLl:PPOLe
- :CRECovery:ZOPLl:SPOLe
Command Syntax
:CRECovery:PLL:EDIRection {RISing | FALLing | BOTH}
Query Syntax
:CRECovery:PLL:EDIRection?
Description
Specifies the signal edge(s) to use when recovering a clock. Typically, for all clock recovery methods except Explicit, you would use BOTH edges of a signal to recover a clock. However, the other options are available if, for example, the signal is a clock signal with a low duty cycle and you want to measure jitter only on its rising (or falling) edges.
Example Command Sequence
:CRECovery:MODE FOPLl :CRECovery:PLL:EDIRection BOTH