:STATus:OPERation:EVENt?

Query Syntax

:STATus:OPERation:EVENt?

Description

Reads and clears the operation event register which contains bits that are set by various reporting registers. These reporting registers are identified in the Bit Definitions section of this topic.

Operation Register Commands
Register Read Write Command
Event ♦   :STATus:OPERation:EVENt?
Enable (mask) ♦ ♦ :STATus:OPERation:ENABle
Operation Status Register Bits
Bit 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0
Bit
Weight
32,768 16,384 8,192 4,096 2,048 1,024 512 256 128 64 32 16 8 4 2 1
Event
Register
— CAL OVLD-ALL OVLD — — LTEST CLIP-ALL CLIP — — — — — TRIG ADER
Enable
Register
                               
Sets to Bit 7 (OPER) of Status Byte Register

Bit Definitions

CAL
A true indicates that an enabled bit in the calibration event status register has been set by a calibration completing
OVLD-ALL
True indicates that an enabled bit in the Overload All event register has been set. Use this when you are using a multiple-oscilloscope system.
OVLD
True indicates that an enabled bit in the Overload event register has been set. Use this when you are using a single-oscilloscope with eight or fewer channels.
LTEST
A true indicates that an enabled bit in the limit test event status register has been set by a limit test completing or failing.
CLIP-ALL
A true indicates that an enabled bit in the Clipped All event status register has been set. Use this when you are using a multiple-oscilloscope system.
CLIP
A true indicates that an enabled bit in the Clipped event status register has been set. Use this when you are using a single-oscilloscope with eight or fewer channels.
TRIG
True indicates that an enabled bit in the Trigger event register has been set.
ADER
True indicates that an enabled bit in the Acquisition Done event register has been set by a completed acquisition.