:SYSTem:TEST
Command Syntax
:SYSTem:TEST [CONNection{1:8}]
When multiple oscilloscopes are connected, you can use the optional [CONNection{1:8}] parameter to identify a particular real-time oscilloscope. Specifying an invalid connection results in the string "Not Present" being returned.
Query Syntax
:SYSTem:TEST? [CONNection{1:8}]
Description
This command begins running instrument self-tests asynchronously. It blocks (acquires *OPC?) until the tests are complete.
You can also use the *TST? (Hardware Self Tests) query to run instrument self tests.
You can cancel a running self test using the :SYSTem:TEST:CANCel command.
The query form, :SYSTem:TEST?, queries self-test logs for the result of the most recent self-test and returns a string in the following format:
"<TimeStamp> <TestName> - Test Status: <Status>"