:SYSTem:TEST:CANCel
Command Syntax
:SYSTem:TEST:CANCel [CONNection{1:8}]
When multiple oscilloscopes are connected, you can use the optional [CONNection{1:8}] parameter to identify a particular real-time oscilloscope. Specifying an invalid connection results in the string "Not Present" being returned.
Description
This command cancels a running self test.
Self tests can be started running using the :SYSTem:TEST command or the *TST? (Hardware Self Tests) query.