:FUNCtion:PARameters:CTLequalizer:ACGain
Command Syntax
:FUNCtionN:PARameters:CTLequalizer:ACGain <AC gain>
<AC gain> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:CTLequalizer:ACGain?
Description
When the Continuous Time Linear Equalizer (CTLE) operator has been selected (:FUNCtion:FOPerator CTLE) and the "2 Pole, AC Gain" CTLE type has been selected (:FUNCtion:PARameters:CTLequalizer:DEFinition P2ACG), the :FUNCtion:PARameters:CTLequalizer:ACGain command specifies the AC Gain as a multiplier value.