:FUNCtion:PARameters:CTLequalizer:BANDwidth

Command Syntax

:FUNCtionN:PARameters:CTLequalizer:BANDwidth <bandwidth>

<bandwidth> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:CTLequalizer:BANDwidth?

Description

In the CUSTom linear Bandwidth Mode (:FUNCtion:PARameters:CTLequalizer:BWMode), this command specifies the linear bandwidth, in Hertz, of a Continuous TimeLinear Equalizer operator (CTLE) (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator CTLE
:FUNCtion2:PARameters:CTLequalizer:BWMode CUSTom
:FUNCtion2:PARameters:CTLequalizer:BANDwidth 8.0E9
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.