:FUNCtion:PARameters:CTLequalizer:PRESets:SELections?
Query Syntax
:FUNCtionN:PARameters:CTLequalizer:PRESets:SELections?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the Continuous Time Linear Equalizer (CTLE) operator. Use the :FUNCtion:PARameters:CTLequalizer:PRESets command to load one of these presets.