:FUNCtion:PARameters:CTLequalizer:GDC

Command Syntax

:FUNCtionN:PARameters:CTLequalizer:GDC{1|2} <low-frequency gain>
            

<low-frequency gain> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:CTLequalizer:GDC{1|2}?

Description

When the Continuous Time Linear Equalizer (CTLE) operator has been selected (:FUNCtion:FOPerator CTLE) and the "2 Pole, 2 Gain" CTLE type has been selected (:FUNCtion:PARameters:CTLequalizer:DEFinition GAIN2), the :FUNCtion:PARameters:CTLequalizer:GDC{1|2} commands specify the DC Gain and DC Gain 2 parameter values in dB.