:FUNCtion:PARameters:CTLequalizer:ZERO

Command Syntax

:FUNCtionN:PARameters:CTLequalizer:ZERO{1|2} <zero_frequency>

<zero_frequency> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:CTLequalizer:ZERO{1|2}?

Description

When the Continuous Time Linear Equalizer (CTLE) operator has been selected (:FUNCtion:FOPerator CTLE) and for most of the selected CTLE types (:FUNCtion:PARameters:CTLequalizer:DEFinition), the :FUNCtion:PARameters:CTLequalizer:ZERO command specifies the zero frequency value(s). The number of zeros for the various CTLE types can be none (in which case, the command is not used), one, or two.

Example Command Sequence

:FUNCtion2:FOPerator CTLequalizer
:FUNCtion2:PARameters:CTLequalizer:GAIN 1.2
:FUNCtion2:PARameters:CTLequalizer:ZERO1 4.0E9
:FUNCtion2:PARameters:CTLequalizer:POLE1 10E9
:FUNCtion2:PARameters:CTLequalizer:POLE2 15.0E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.