:FUNCtion:PARameters:CTLequalizer:FZP
Command Syntax
:FUNCtionN:PARameters:CTLequalizer:FZP <low-frequency zero-pole>
<low-frequency zero-pole> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:FUNCtionN:PARameters:CTLequalizer:FZP?
Description
When the Continuous Time Linear Equalizer (CTLE) operator has been selected (:FUNCtion:FOPerator CTLE) and the "2 Pole, 2 Gain" CTLE type has been selected (:FUNCtion:PARameters:CTLequalizer:DEFinition GAIN2), the :FUNCtion:PARameters:CTLequalizer:FZP command specifies the low-frequency zero/pole frequency in Hertz.