:LTESt:ACQuire:SWAVeform:CMODe{N}:STATe

Command Syntax

:LTESt:ACQuire:SWAVeform:CMODeN:STATe {DISK | MEMory | OFF}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:LTESt:ACQuire:SWAVeform:CMODeN:STATe?

Query Response

{DISK | MEM | OFF}

Description

Selects to save a common-mode waveforms to a file or memory after the limit test acquires the specified number of waveforms, samples, or patterns. Use the :LTESt:ACQuire:CTYPe command and its child commands to specify the test conditions required to end the test. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command. The following command arguments are available:

DISK
Saves the waveform to a file. Use the :LTESt:ACQuire:SWAVeform:CMODe{N}:FNAMe command to specify the file name.
MEMory
Saves the waveform to a memory location. Use the :LTESt:ACQuire:SWAVeform:CMODe{N}:WMEMory WMEMory{1:8} command to specify the memory location.
OFF
Turns off the saving of a common-mode waveform.