:LTESt:ACQuire:SWAVeform:CMODe{N}:WMEMory WMEMory{1:8}
Command Syntax
:LTESt:ACQuire:SWAVeform:CMODeN:WMEMory
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:LTESt:ACQuire:SWAVeform:CMODeN:WMEMory?
Description
Specifies a waveform memory for saving a common-mode waveform as a reporting action for an acquisition limit test. Use the :LTESt:ACQuire:SWAVeform:CMODe{N}:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.