:LTESt:ACQuire:SWAVeform:DIFF{N}:WMEMory
Command Syntax
:LTESt:ACQuire:SWAVeform:DIFF{N}:WMEMory WMEMory{1:8}
{N} identifies the differential waveform, which must be selected from "<connection1-8>_<ch1,3,5,7>". For example, the differential waveform of connection 4 channels 1 and 2 would be identified as DIFF4_1.
Query Syntax
:LTESt:ACQuire:SWAVeform:DIFF{N}:WMEMory?
Description
Specifies a waveform memory for saving a differential waveform as a reporting action for an acquisition limit test. Use the :LTESt:ACQuire:SWAVeform:DIFF{N}:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.