:LTESt:ACQuire:SWAVeform:DIFF{N}:STATe
Command Syntax
:LTESt:ACQuire:SWAVeform:DIFF{N}:STATe {DISK | MEMory | OFF}
{N} identifies the differential waveform, which must be selected from "<connection1-8>_<ch1,3,5,7>". For example, the differential waveform of connection 4 channels 1 and 2 would be identified as DIFF4_1.
Query Syntax
:LTESt:ACQuire:SWAVeform:DIFF{N}:STATe?
Query Response
{DISK | MEM | OFF}
Description
Selects to save a differential waveform to a file or memory after the limit test acquires the specified number of waveforms, samples, or patterns. Use the :LTESt:ACQuire:CTYPe command and its child commands to specify the test conditions required to end the test. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command. The following command arguments are available:
- DISK
- Saves the waveform to a file. Use the
:LTESt:ACQuire:SWAVeform:DIFF{N}:FNAMecommand to specify the file name. - MEMory
- Saves the waveform to a memory location. Use the
:LTESt:ACQuire:SWAVeform:DIFF{N}:WMEMorycommand to specify the memory location. - OFF
- Turns off the saving of a differential waveform.