:LTESt:ACQuire:SWAVeform:FUNCtion{N}:WMEMory

Command Syntax

:LTESt:ACQuire:SWAVeform:FUNCtion{1:64}:WMEMory WMEMory{1:8}

Query Syntax

:LTESt:ACQuire:SWAVeform:FUNCtion{1:64}:WMEMory?

Description

Specifies a waveform memory for saving a function waveform as a reporting action for an acquisition limit test. Use the :LTESt:ACQuire:SWAVeform:FUNCtion{N}:STATe command to enable and disable waveform reporting for the channel. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.