:LTESt:LLINe:SWAVeform:CHANnel{N}:WMEMory

Command Syntax

:LTESt:LLINe:SWAVeform:CHANnel{N}:WMEMory WMEMory{1:8}

{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:LTESt:LLINe:SWAVeform:CHANnel{N}:WMEMory?

Description

Upon completion of limit testing for a limit line test, any channel waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific channel. To actually enable channel waveforms to be saved, use the :LTESt:LLINe:SWAVeform:CHANnel{N}:STATe command.

To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST{N}:STATe command.