:LTESt:LLINe:SWAVeform:DIFF{N}:WMEMory

Command Syntax

:LTESt:LLINe:SWAVeform:DIFF{N}:WMEMory WMEMory{1:8}

{N} identifies the differential waveform, which must be selected from "<connection1-8>_<ch1,3,5,7>". For example, the differential waveform of connection 4 channels 1 and 2 would be identified as DIFF4_1.

Query Syntax

:LTESt:LLINe:SWAVeform:DIFF{N}:WMEMory?

Description

Upon completion of limit testing for a limit line test, any differential waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific differential waveform. To actually enable differential waveforms to be saved, use the :LTESt:LLINe:SWAVeform:DIFF{N}:STATe command.

To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST{N}:STATe command.