:LTESt:LLINe:SWAVeform:CMODe{N}:WMEMory
Command Syntax
:LTESt:LLINe:SWAVeform:CMODeN:WMEMory WMEMory{1:8}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:LTESt:LLINe:SWAVeform:CMODeN:WMEMory?
Description
Upon completion of limit testing for a limit line test, any common-mode waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific common-mode waveform. To actually enable common-mode waveforms to be saved, use the :LTESt:LLINe:SWAVeform:CMODe{N}:STATe command.
To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST{N}:STATe command.