:LTESt:LLINe:SWAVeform:CMODe{N}:STATe

Command Syntax

:LTESt:LLINe:SWAVeform:CMODeN:STATe {DISK | MEMory | OFF}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:LTESt:LLINe:SWAVeform:CMODeN:STATe?

Description

Specifies the reporting action for the selected common-mode waveforms upon completion of limit testing for a limit line test. Use the command argument to select or turn off the reporting action. To disable the reporting action of all channel, common-mode, differential, and function waveforms, use the :LTESt:LLINe:SWAVeform:RESet command.

To turn on limit testing for a limit line test, use the :LTESt:LLINe:TEST{N}:STATe command.

Command Arguments
Argument Description
DISK Saves the waveform to a file (.h5) in the %USER_DATA_DIR%\Limit Lines folder. Use the :LTESt:LLINe:SWAVeform:CMODe{N}:FNAMe command to specify the file name.
MEMory Saves the waveform to a memory location. Use the :LTESt:LLINe:SWAVeform:CMODe{N}:WMEMory command to specify the memory location.
OFF Turns off the saving of a common-mode waveform.