:LTESt:LLINe:SWAVeform:RESet

Command Syntax

:LTESt:LLINe:SWAVeform:RESet

Description

Turns off the reporting action to save channel, differential, common-mode, and function waveforms to a file or memory location whenever limit testing for a limit line test stops data acquisition. It is equivalent to sending the following command for each available waveform:

:LTESt:LLINe:SWAVeform:CHANnel:STATe OFF
:LTESt:LLINe:SWAVeform:CMODe:STATe OFF
:LTESt:LLINe:SWAVeform:DIFF:STATe OFF
:LTESt:LLINe:SWAVeform:FUNCtion:STATe OFF