:LTESt:MEASure:SWAVeform:CMODe{N}:STATe
Command Syntax
:LTESt:MEASure:SWAVeform:CMODeN:STATe {DISK | MEMory | OFF}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:LTESt:MEASure:SWAVeform:CMODeN:STATe?
Query Response
{DISK | MEM | OFF}
Description
Saves a common-mode waveform to a file or memory location after the measurement limit test acquires the specified number of failures. The following command arguments are available:
- DISK
- Saves the waveform to a file. Use the
:LTESt:MEASure:SWAVeform:CMODe{N}:FNAMecommand to specify the file name. - MEMory
- Saves the waveform to a memory location. Use the
:LTESt:MEASure:SWAVeform:CMODe{N}:WMEMorycommand to specify the memory location. - OFF
- Turns off the saving of a common-mode waveform.