:LTESt:MEASure:SWAVeform:DIFF{N}:WMEMory

Command Syntax

:LTESt:MEASure:SWAVeform:DIFF{N}:WMEMory WMEMory{1:8}

{N} identifies the differential waveform, which must be selected from "<connection1-8>_<ch1,3,5,7>". For example, the differential waveform of connection 4 channels 1 and 2 would be identified as DIFF4_1.

Query Syntax

:LTESt:MEASure:SWAVeform:DIFF{N}:WMEMory?

Description

Upon completion of an measurement limit test, selects a waveform memory as a destination to save a differential waveform. Use the :LTESt:MEASure:SWAVeform:DIFF{N}:STATe command to enable and disable waveform reporting for the channel. Use the :LTESt:MEASure:MLIMit:STATe command to turn off the measurement limit test