:LTESt:MEASure:SWAVeform:CHANnel{N}:STATe

Command Syntax

:LTESt:MEASure:SWAVeform:CHANnel{N}:STATe {DISK | MEMory | OFF}

CHANnel{N} identifies the channel as in CHANnel1_1, CHANnel1_2, …, CHANnel8_8.

Query Syntax

:LTESt:MEASure:SWAVeform:CHANnel{N}:STATe?

Query Response

{DISK | MEM | OFF}

Description

Saves a channel waveform to a file or memory location after the measurement limit test acquires the specified number of failures. The following command arguments are available:

DISK
Saves the waveform to a file. Use the :LTESt:MEASure:SWAVeform:CHANnel{N}:FNAMe command to specify the file name.
MEMory
Saves the waveform to a memory location. Use the :LTESt:MEASure:SWAVeform:CHANnel{N}:WMEMory command to specify the memory location.
OFF
Turns off the saving of a common-mode waveform.